Press Release

Contact Sarah Shieh

High Common-Mode Voltage Difference Amplifier Enables Direct Interface to High Voltage Input up to ±600 V

May 3 2013 - Norwood, MA
  • Analog Devices, Inc. (ADI) today introduced the industry’s first precision difference amplifier to maintain excellent Common-Mode Rejection Ratio (CMRR) that exceeds 90dB at voltages up to ±600 V. Designed for applications such as motor control, process control and power supplies, the AD8479 enables accurate measurements of currents in the presence of voltage fluctuations as large as ±600 V without additional complex signal conditioning components.

    The AD8479 guarantees to reject ±200V with ±5V power supplies. The AD8479 offers cost-effective isolation and can replace more costly devices in applications that do not require galvanic isolation. With higher than 90 dB CMRR, 130 kHz bandwidth, 2MΩ differential input impedance, within 0.02% gain error and 5ppm/°C gain drift, the AD8479 offers precision over a wide range of common-mode voltages and frequencies. It operates over an extended temperature range of -40°C to +125°C.

    • View the AD8479 product pages, download the data sheet and order samples.
    • Get your questions answered by ADI engineers on EngineerZone®, ADI’s online technical support community

     Sample Availability
     Full Production
     Price Each in
    1,000 Quantities

  • About Analog Devices
  • Innovation, performance, and excellence are the cultural pillars on which Analog Devices has built one of the longest standing, highest growth companies within the technology sector. Acknowledged industry-wide as the world leader in data conversion and signal conditioning technology, Analog Devices serves over 60,000 customers, representing virtually all types of electronic equipment. Analog Devices is headquartered in Norwood, Massachusetts, with design and manufacturing facilities throughout the world. Analog Devices is included in the S&P 500 Index.
  • To subscribe to Analog Dialogue, ADI's monthly technical journal, visit:
  • Editor's Contact Information
Stay Informed