Press Release

Contact Grainne Murphy

Analog Devices’ Data Acquisition IC Simplifies Industrial and Instrumentation Equipment Design

ADI’s ADAS3022 integrates a complete precision data acquisition analog signal chain in a single integrated circuit.

Nov 13 2012 - Norwood, MA
  • Analog Devices, Inc. (ADI), the global leader in data-conversion technology*, today introduced a highly integrated data acquisition IC (integrated circuit) that uses one-third the board space of competing discrete devices to help engineers simplify the design and reduce the size of advanced industrial data acquisition systems. The new 16-bit, 1-MSPS (million-samples-per-second) ADAS3022 data acquisition IC is effective for power-line monitors, process and motor control, patient monitoring, and other industrial and instrumentation systems that operate within the ±10 V industrial range.

    "With a dominant global data conversion market share of approximately 48.5 percent in 2011, Analog Devices is considered by Databeans as the guiding force in the cutting edge data acquisition and signal conditioning market. With unique new products such as the ADAS3022, which promises very high performance in a smaller form factor, Analog Devices remains responsible for many of the high-level advancements that drive this dynamic industry forward,” said Matthew Scherer, market analyst, Databeans Inc. “As a result of such product releases, Databeans believe that Analog Devices is well positioned to remain the dominant player in this market for years to come."

    The ADAS3022 data acquisition IC integrates ADI’s 16-bit PulSAR® successive-approximation A/D converter core with high-impedance input buffers and a 7-stage on-chip PGIA (programmable-gain instrumentation amplifier). The ADAS3022 includes an 8-channel, low-leakage multiplexer and precision low-drift 4.096-V reference. With eight data channels and delivering full 16-bit dynamic range, the new IC is optimized to interface with a wide range of sensors running from ±10 V to as low as ±640 mV.

    The ADAS3022 offers a complete factory calibrated and tested signal chain. This addresses the settling time, signal buffering, level shifting, noise amplification/rejection and other analog signal-conditioning challenges that were once a standard part of the system design process

    Recommended Complementary Components

    Complementary components for the ADAS3022 include the ADR381 band gap voltage reference, ADR434x XFET voltage reference, ADR454x ultra-low-noise voltage reference, ADP1613/14 step-up PWM switching converter, ADP1715 linear regulator, ADP3334 linear regulator, ADP7102/04 CMOS low-noise LDO, AD8031/32 low power reference buffer, and ADA4841 low power ADC drivers for auxiliary input pair (AUX±). An evaluation board is also available that allows system designers to configure the ADAS3022 without engaging in circuit-board design or writing software code.

    Pricing and Availability

    Product Sampling Temperature Range Price Each Per 1,000 Packaging
    ADAS3022 Now -40°C to +85°C $14.95 6 mm x 6 mm 40-lead LFCSP ((lead-frame chip-scale package)

    • Download data sheet, view product page, and request samples: ADAS3022
    • Get support at ADI’s EngineerZone™ online technical support community
  • About Analog Devices
  • Innovation, performance, and excellence are the cultural pillars on which Analog Devices has built one of the longest standing, highest growth companies within the technology sector. Acknowledged industry-wide as the world leader in data conversion and signal conditioning technology, Analog Devices serves over 60,000 customers, representing virtually all types of electronic equipment. Analog Devices is headquartered in Norwood, Massachusetts, with design and manufacturing facilities throughout the world. Analog Devices is included in the S&P 500 Index.
  • Editor's Contact Information
Stay Informed