Press Release

Contact Bob Olson

Analog Devices' FMC Boards Support Xilinx's FPGA Targeted Design Platforms to Help Designers Reduce Development Time

ADI's A/D and D/A converter FPGA mezzanine cards include all HDL code and device drivers for easy integration with multiple generations of Xilinx FPGAs.

Jan 31 2012 - Norwood, MA
  • Analog Devices, Inc. (ADI), the leading provider of data conversion technology*, today introduced two data converter FMC boards (FPGA mezzanine cards) that connect to Xilinx Inc.'s new 28nm 7 series FPGA (field programmable gate array) evaluation kits. ADI's high-speed AD9739A D/A converter and AD9467 A/D converter FMC boards support multiple generations of Xilinx kits -- including the company's new Kintex-7 FPGA evaluation kits Xilinx announced today. The new Analog Devices FMC boards include all of the HDL (hardware description language) code and device drivers needed for designers to engage in rapid prototyping and reduce development time and risk. Both products are being demonstrated at the DesignCon 2012 trade show in Santa Clara, Calif., in the Xilinx booth (#732).

    "The availability of low cost commercial off the shelf hardware, such as the AD9739A FMC board, and the new Kintex-7 development boards, allows our customers to quickly prototype and evaluate many of the IP Cores which we offer," said Jean-Claude Basset, technical director/manager, MVD Cores**, a Certified Member of the Xilinx Alliance Program. "We have verified our digital RF up converter IP cores with the AD9739A FMC board and Xilinx's Virtex-6, Kintex-7 and Spartan-6 boards and recommend that our customers use this hardware to evaluate our IP Cores."

    "ADI's new FMC boards, integration software and industry-leading data conversion expertise help engineers designing with Xilinx’s Kintex-7 series FPGAs to move more quickly through system prototyping and get their products to market faster," said Dave Babicz, director of Global Alliances, Analog Devices. "At the same time, our new boards are backward compatible with other Xilinx FPGAs, which means that engineers will be able to design products that meet a range of performance criteria using a simplified design environment."

    "Xilinx's Targeted Design Platforms accelerate system development and integration by providing the industry's most comprehensive development kits, which include boards, tools, IP cores, reference designs and FMC support," said Raj Seelam, senior marketing manager, Targeted Design Platforms, Xilinx. "Our adoption and support for open standards such as FMC and the AMBA®4 AXI IP core interface strengthens the ability of Xilinx Alliance Program members like Analog Devices to deliver key technologies that make it easier for FPGA users to complete their projects."

    More About ADI's AD9739A D/A Converter FMC Board

    ADI's AD9739A FMC board is based on the AD9739A, a 14-bit D/A converter that enables cable television and broadband operators to synthesize the entire cable spectrum up to 1 GHz into a single RF (radio frequency) port, while consuming a maximum of 1.1 W of power. The AD9739A 14-bit, 2.5-GSPS D/A converter's wide bandwidth and dynamic range enable cable operators to increase the QAM (quadrature amplitude modulation) channel densities by 20 times over the densities found in today’s cable modems. Competing D/A converter solutions require an additional 28 LVDS (low-voltage differential signaling) pairs for the data interface.

    More About ADI's AD9467 A/D Converter FMC Board

    ADI's AD9467 FMC board is based on the AD9467, which is a 16-bit, 250-MSPS A/D converter that operates on 35 percent less power at a 25 percent higher sampling rate than any other 16-bit data converter. The AD9467 provides a new level of signal processing performance for test and measurement instrumentation, defense electronics and communications applications where high resolution over a wide bandwidth is needed.

    The AD9467 delivers resolution and a fast sample rate while simultaneously achieving a high SFDR (spurious-free dynamic range) of up to 100 dBFS and SNR (signal-to-noise ratio) performance of 76.4 dBFS. The device’s SFDR of 90 dBFS up to 300 MHz analog input and 60-femtosecond rms (root mean square) jitter help lower the signal chain bill of materials component count by allowing engineers to increase system performance at higher intermediate frequencies, thereby reducing the number of signal down-conversion stages.

    Availability and Pricing

    Product Availability Price
    AD9739A FMC board with 14-bit D/A converter Now $349
    AD9467 FMC board with 16-bit A/D converter March 2012 Contact Digilent Inc.

  • $name
  • Editor's Contact Information
Stay Informed