Press Release

About The Author
Joe Dussi ,

Analog Devices Unveils Ultra-Low-Power Boost Regulator for Energy Harvesting Systems

ADI’s ADP5090 offers low-light power conversion and multiple power path management capability.

Apr 1 2014 - Norwood, MA
  • Analog Devices, Inc. (NASDAQ: ADI) introduced today the industry’s most efficient ultra-low-power boost regulator for photovoltaic and thermoelectric energy harvestingsystems.The ADP5090 ultra-low-power boost regulator represents a significant leap forward in energy harvesting technology by delivering efficient conversion of the harvested power (as low as 10 uW) with sub-uW operational losses that stores the maximum amount of energy for future operation. Harnessing “indoor” ambient light as a viable power source has become a growing trend in wireless sensor network applications worldwide.

    • Download ADP5090 data sheet, user guide or order samples
    • Connect with ADI engineers on EngineerZone™, an online technical support community
    • Learn about ADI’s offerings for building technology products


    ADP5090 Ultra-Low-Power Boost Regulator Key Features


    • Optimizes efficient conversion of harvested limited power down to 10 µW – 1-mW range with best in class sub-µW operation losses
    • Programmable maximum power point tracking with open circuit voltage sensing ensures most energy extracted from harvester
    • 250-nA quiescent current in deep-sleep mode prolongs operation time with minimized loss of ambient energy
    • Integrated charge pump circuitry enables cold start at 380-mV input voltage with no energy on system node


    Pricing and Availability

    Product
    Availability
    Price Each per 1,000
    Package
    ADP5090
    Now
    $2.50
    3-mm x 3-mm 16-lead LFCSP
  • About Analog Devices
  • Innovation, performance, and excellence are the cultural pillars on which Analog Devices has built one of the longest standing, highest growth companies within the technology sector. Acknowledged industry-wide as the world leader in data conversion and signal conditioning technology, Analog Devices serves over 60,000 customers, representing virtually all types of electronic equipment. Analog Devices is headquartered in Norwood, Massachusetts, with design and manufacturing facilities throughout the world. Analog Devices is included in the S&P 500 Index.
  • EngineerZone is a trademark of Analog Devices, Inc.

    To subscribe to Analog Dialogue, ADI's monthly technical journal, visit: http://www.analog.com/subscribe


  • Editor's Contact Information
Stay Informed