Press Release

About The Author
Grainne Murphy ,

353-61-495540

Released Today: Industry’s Lowest Power 18-bit SAR A/D Converters

AD7989-1 and AD7989-5 PulSAR ® A/D converters provide low power, high precision solutions for portable applications.

6 Mar 14 - Norwood, MA
  • Analog Devices, Inc. (NASDAQ: ADI) introduced today two 18-bit A/D converters that combine the industry’s lowest power with excellent accuracy. The AD7989-1 and AD7989-5 PulSAR ® A/D converters consume 400 µW at 100 kSPS. Power consumption is scaled depending on throughput speed to address thermal dissipation challenges in dense data acquisition system designs. The A/D converters feature +/-1 LSB and 98 dB SNR at 1 kHz for high dynamic range with exceptional accuracy and precision. Both A/D converters are available in 100 kSPS and 500 kSPS throughput options, incorporate a low power, high precision, 18-bit sampling A/D converter and a versatile serial interface port.

    The AD7989-1 and AD7989-5 PulSAR® A/D converters are the newest additions to Analog Devices’ PulSAR portfolio. The PulSAR portfolio includes 18- and 16-bit A/D precision converters ranging from 100 kSPS to 1 MSPS. They provide a versatile pin-compatible upgrade/downgrade path for performance in a wide range of markets including battery-powered equipment, data acquisition systems and medical instrumentation.

    • Download AD7989-1 data sheet, order samples and evaluation boards.
    • Pin-compatible 500 kSPS AD7989-5 option.
    • Connect with engineers and ADI product experts on EngineerZone™, an online technical support community

    Pricing, Availability and Complementary Products

     Product Sample/Full Production
    Availability 
    Resolution  Speed Price Each Per
    1,000
    Packaging
     AD7989-1
     NOW
     18-bit
     100 kSPS
     $8.55
     3 mm x 3 mm 10-lead LFCSP or 10-lead MSOP
     AD7989-5
     NOW
     18-bit
     500 kSPS
     $11.95
     3 mm x 3 mm 10-lead LFCSP or10-lead MSOP


    These A/D converters can be designed into data acquisition circuits with ADI’s high precision amplifiers and references such as the low-power, low-noise, low-distortion ADA4841-2 and ADR434.


  • About Analog Devices
  • Innovation, performance, and excellence are the cultural pillars on which Analog Devices has built one of the longest standing, highest growth companies within the technology sector. Acknowledged industry-wide as the world leader in data conversion and signal conditioning technology, Analog Devices serves over 60,000 customers, representing virtually all types of electronic equipment. Analog Devices is headquartered in Norwood, Massachusetts, with design and manufacturing facilities throughout the world. Analog Devices is included in the S&P 500 Index.
  • To subscribe to Analog Dialogue, ADI's monthly technical journal, visit: http://www.analog.com/subscribe
  • Editor's Contact Information
Stay Informed