Press Release

About The Author
Joe Dussi ,

Ultra-Low-Noise RF Low-Dropout Regulators Reduce Phase Noise in Wideband Communication Systems

Reduces LDO noise spectral density by a factor of two
Provides lowest phase noise for powering VCOs; lowest jitter performance for powering clock devices in microwave systems

6 Nov 13 - Norwood, MA
  • Analog Devices, Inc. (NASDAQ: ADI), a global leader in high-performance semiconductors for signal processing applications, announced today the release of ultra-low-noise LDO (low-dropout) regulators for RF (radio frequency) signal devices. The ADM7150/1 operate from 4.5 V to 16 V, provide up to 800-mA of output current and support output voltages from 1.5 to 5.0 V. The LDOs achieve an output-NSD (noise spectral density) of 1.4 nV/rtHz from 10 kHz to 1 MHz, which significantly reduces VCO (voltage-controlled oscillator) phase noise in point-to-point microwave radios, satellite communications, defense electronics and other wideband applications. Additionally, a user adjustable CBYP can significantly reduce low frequency 1/f noise (8 nV/rtHz at 100 Hz) for precision analog front-end measurement systems.


    In addition to ultra-low noise, the ADM7150/1 achieve line and load transient responses of 0.01%/V and 0.4%/A respectively with a 10-µF ceramic output capacitor. The new LDOs also feature high PSRR (power-supply rejection ratio) performance of greater than 90 dB from 1 kHz to 100 kHz, and greater than 60 dB at 1 MHz. This effectively filters DC-DC switching regulator ripple, saving space by minimizing the size of discrete filtering components normally needed.

    Pricing, Availability and Complementary Products

    Product
    Availability  Price (1K units)  Package 
    ADM7150(fixed Vout Now $3.64  3-mm x 3-mm 8-lead LFCSP and SOIC 
    ADM7151(adj Vout Now  $3.64  3-mm x 3-mm 8-lead LFCSP and SOIC 
    ADM7160  Now  $0.96  2-mm x 2-mm LFCSP and TSOT-5 
  • About Analog Devices
  • Innovation, performance, and excellence are the cultural pillars on which Analog Devices has built one of the longest standing, highest growth companies within the technology sector. Acknowledged industry-wide as the world leader in data conversion and signal conditioning technology, Analog Devices serves over 60,000 customers, representing virtually all types of electronic equipment. Analog Devices is headquartered in Norwood, Massachusetts, with design and manufacturing facilities throughout the world. Analog Devices is included in the S&P 500 Index.
  • To subscribe to Analog Dialogue, ADI’s monthly technical journal, visit: http://www.analog.com/library/analogDialogue/
  • Editor's Contact Information
Stay Informed