Press Release

About The Author
Joe Dussi ,

Isolated Error Amplifiers Outperform Optocouplers and Shunt Regulators in Power Supply Applications

26 Feb 13 - Norwood, MA
  • Analog Devices, Inc. (NASDAQ: ADI), a global leader in high-performance semiconductors for signal-processing applications and a pioneer in digital isolator technology, today introduced isolated error amplifiers that provide power supply designers with a higher performing, single-chip alternative to isolation techniques based on optocouplers and shunt regulators. Designed for linear feedback power supplies using primary side controllers, the ADuM3190 and ADuM4190 isolated error amplifiers have a 400-kHz bandwidth, with 0.5% typical initial accuracy at 25°C and 1% total accuracy over the extended temperature range of –40˚C to +125˚C. This provides manufacturers of ac-to-dc and dc-to-dc power supplies, including those that are DOSA (Distributed-power Open Standards Alliance)-compliant, with a significant upgrade in speed and operating temperature range, as well as a 5× improvement in transient response. 

    Designed with ADI’s iCoupler® digital isolation technology, the ADuM3190 and ADuM4190 eliminate the CTR (current-transfer ratio) of optocouplers that degrades over the lifetime of the devices and limits operation to 85˚C. The ADuM3190 and ADuM4190 include a highly accurate 1.225-V reference and a wideband operational amplifier that can be used to set up a variety of commonly used power supply loop compensation techniques. 

    ADuM3190/4190 Isolated Error Amplifiers Key Features 

    • Bandwidth: 400 kHz
    • 0.5% initial accuracy at 25°C
    • 1% total accuracy over –40˚C to +125˚C
    • Low power operation: <7 mA
    • Isolation voltage:
      • ADuM3190: 2.5 kV rms
      • ADuM4190: 5 kV rms (reinforced)


    Pricing and Availability

    Product
    Availability
    Price at 1K Quantity
    Package
    Temperature Range (°C) 
     ADuM3190A
     Now
     $1.04
     QSOP-16
     –40 to +85
     ADuM3190B
     Now
     $1.12
     QSOP-16
     –40 to +85
     ADuM3190S
     Now
     $1.14
     QSOP-16
    –40 to +125
     ADuM3190T
     Now
     $1.23
     QSOP-16
     –40 to +125
     ADuM4190A
     April '13
     $1.20
     Wide-body SO-16
     –40 to +85
     ADuM4190S
     April '13
     $1.30
     Wide-body SO-16
     –40 to +125
     ADuM4190T
     April '13
     $1.39
     Wide-body SO-16
     –40 to +125
     EVAL-ADUM3190EBZ
     Now
     $49 per
     -  -

  • About Analog Devices
  • Innovation, performance, and excellence are the cultural pillars on which Analog Devices has built one of the longest standing, highest growth companies within the technology sector. Acknowledged industry-wide as the world leader in data conversion and signal conditioning technology, Analog Devices serves over 60,000 customers, representing virtually all types of electronic equipment. Analog Devices is headquartered in Norwood, Massachusetts, with design and manufacturing facilities throughout the world. Analog Devices is included in the S&P 500 Index.
  • EngineerZone is a registered trademark of Analog Devices, Inc.

    Subscribe to Analog Dialogue, ADI’s monthly technical journal: http://www.analog.com/library/analogDialogue/

  • Editor's Contact Information
Stay Informed