Press Release

About The Author
Sarah Shieh ,

New Release of the Free Analog Devices SPICE Simulation Tool Visualizes and Enhances Component Evaluation for Linear Designs

Jun 27 2012 - Norwood, MA
  • Analog Devices, Inc. (ADI) today announced a new release of the NI Multisim™ Component Evaluator – Analog Devices® Edition. In collaboration with National Instruments Corp. (NI), the new version of the free tool adds features and functionality to provide engineers with an easy-to-use environment for the simulation of linear circuits using ADI components. The new release of the Multisim – ADI Edition includes more than 870 models of ADI’s linear components. By pairing these components with intuitive simulation features and SPICE analyses, engineers can now visualize and evaluate linear performance, making this critical step of circuit design easier, faster and far more productive. The free component evaluation tool is available for download on ADI’s website at http://www.analog.com/multisim.

    The Multisim – ADI Edition allows engineers to design larger, more complex circuits and import their own models into the tool. The new Multisim snippets feature allows engineers to “drag and drop” saved Multisim circuit files for sharing or to use in new designs. The new tool release further enhances the user experience with virtual component property editing and provides a highly graphical environment for advanced simulation features and analyses, making it easier than ever for designers to build and evaluate complete linear circuits.

  • About Analog Devices
  • Innovation, performance, and excellence are the cultural pillars on which Analog Devices has built one of the longest standing, highest growth companies within the technology sector. Acknowledged industry-wide as the world leader in data conversion and signal conditioning technology, Analog Devices serves over 60,000 customers, representing virtually all types of electronic equipment. Analog Devices is headquartered in Norwood, Massachusetts, with design and manufacturing facilities throughout the world. Analog Devices is included in the S&P 500 Index.
  • Editor's Contact Information
Stay Informed