Press Release

About The Author
Doug Bartow ,

Analog Devices' nanoDAC+™ Converters Offer Industry's Best D/A Converter Performance and Smallest Packages

ADI’s AD568xR nanoDAC+™ converter series features quad D/A converters with choice of 16, 14 or 12 bits of resolution in tiny packages for a wide range of instrumentation and communications applications.

2 May 12 - Norwood, MA
  • Analog Devices, Inc., (NASDAQ: ADI) the data converter market share leader*, today introduced a series of quad 16-, 14- and 12-bit D/A converters in space-saving 16-lead surface-mount LFCSP or leaded TSSOP packages. ADI’s new AD568xR nanoDAC+™ series of quad D/A converters has the industry’s best DC performance (INL, offset error and gain error) and smallest package size, with a choice of on-chip or external reference and SPI or I²C control interface. Applications such as PLC I/O cards, digital oscilloscopes, signal generators and optical modules that require low power, rail-to-rail, single-supply D/A converters will benefit from the AD568xR series’ industry leading performance.

    “Customers, who previously had to trade off board area to achieve higher levels of digital-to-analog accuracy and reference drift performance now have a solution that meets all of their requirements,” said Donal Geraghty, director of Precision D/A Converters, Analog Devices. “The AD5686R delivers four D/A converters with 16-bit accuracy and a 2-ppm/°C reference in a tiny 3mm x 3mm package.”

    AD5686R Quad D/A Converter Features and Benefits:

    Pricing, Availability and Complementary Products

    Samples and evaluation board are currently available.

    Product Availability Resolution (Bits) Interface Price
    AD5686R Now 16 SPI $8.06
    AD5696R Now 16 I2C $8.06
    AD5685R Now 14 SPI $5.76
    AD5695R Now 14 I2C $5.76
    AD5684R Now 12 SPI $4.80
    AD5694R Now 12 I2C $4.80

    Complementary components include ADI’s AD5750-2 which is a single-channel, low cost, precision voltage/current output driver amplifier, ideally suited for use with the AD5686R in PLC I/O card applications.

  • About Analog Devices
  • Innovation, performance, and excellence are the cultural pillars on which Analog Devices has built one of the longest standing, highest growth companies within the technology sector. Acknowledged industry-wide as the world leader in data conversion and signal conditioning technology, Analog Devices serves over 60,000 customers, representing virtually all types of electronic equipment. Analog Devices is headquartered in Norwood, Massachusetts, with design and manufacturing facilities throughout the world. Analog Devices is included in the S&P 500 Index.
  • Editor's Contact Information
Stay Informed