Press Release

About The Author
Linda Kincaid ,

(781) 937-1472

Multi-channel Energy Measurement Chip Provides Flexibility and Scalability for Broad Range of Monitoring Applications

21 Mar 12 - Norwood, MA
  • Analog Devices, Inc., (ADI) a global leader in high-performance semiconductors for signal processing applications, today introduced a single-chip energy measurement AFE (analog front end) that monitors the energy consumption and power quality of up to six electrical circuits. The ADE7816 energy measurement AFE is designed for data center power distribution units, energy monitoring and management systems, and multi-channel electricity meters. Able to measure one voltage and up to six current channels, the new AFE provides high-accuracy energy usage and power quality data for each circuit. Since it interfaces to standard microcontrollers, the ADE7816 energy measurement AFE is specifically suited for applications that require more processor flexibility and peripheral options than is offered by fixed-configuration SOC (system-on-chip) devices. Additionally, multiple ADE7816 energy measurement AFEs can interface with a single application processor resulting in scalable and cost-effective solutions.

    ADE7816 Energy Measurement AFE Key Features

    Pricing and Availability

    Product Sample Availability Full-Volume Production Price Each in 1,000 Quantities Package
    ADE7816 Now Now $6.35 40-lead LFCSP (lead frame chip scale package)

    Making a Difference for Energy Metering Customers

    With more than 350 million energy meters using ADI’s technology deployed worldwide, Analog Devices has delivered more energy measurement solutions than any other semiconductor company. Superior in quality, reliability, and performance, Analog Devices’ energy-metering ICs combine ADCs (analog-to-digital converters) with fixed-function DSPs (digital signal processors) to perform critical measurements, while providing unparalleled functionality and ease-of-use. Analog Devices offers a broad range of semiconductor solutions that solve design challenges in every aspect of metering systems, including energy measurement; data and power management; user interface; and RF, GSM/GPRS, and power-line carrier communication solutions. For more information about ADI’s energy measurement products, visit http://www.analog.com/pr/Energy-Measurement. For more information about ADI’s energy solutions for renewable energy generation, transmission and distribution, and metering applications, visit www.analog.com/energy.

    • View the ADE7816 energy measurement AFE product page, order samples, and download the data sheet: http://www.analog.com/ADE7816.
    • Supports flexible system design by interfacing a wide variety of user-selectable microcontroller configurations
    • Enables scalable system design by using multiple ADE7816 AFEs with a single application MCU (microcontroller)
    • Flexible system design supports shunts, Rogowski coils and current transformers
    • Flexible I2C, SPI (serial port interface) and HSDC (high-speed data capture) provide access to real-time raw waveform samples
    • Saves board space and cost by replacing up to six, single-phase energy metering ICs (integrated circuits)
    • Uses ADI’s field-proven, revenue-grade measurements that include active and reactive energies, instantaneous rms voltage and currents
    • Saves development time by integrating power quality information, including over-voltage, over-current, peak and sag detection
    • Provides industry leading less than 0.2 percent error in active and reactive energy over a dynamic range of 3000:1 and meets accuracy requirements of Class 0.5 revenue-grade electricity meters
  • About Analog Devices
  • Innovation, performance, and excellence are the cultural pillars on which Analog Devices has built one of the longest standing, highest growth companies within the technology sector. Acknowledged industry-wide as the world leader in data conversion and signal conditioning technology, Analog Devices serves over 60,000 customers, representing virtually all types of electronic equipment. Analog Devices is headquartered in Norwood, Massachusetts, with design and manufacturing facilities throughout the world. Analog Devices is included in the S&P 500 Index.
  • Editor's Contact Information
Stay Informed