SUPPLEMENTAL RESOURCES - CN0164: Low Power, Long Range, ISM Wireless Measuring Node

Application Notes (10)
Circuit Note (9)
Technical Articles (10)
ADIsim Design/Simulation Tools (3)
Code Examples (2)
Data Sheets (3)
Design Calculators (1)
Documentation (11)
Evaluation Software (1)
  • ADF70xx Evaluation Software  (zip, 24777 kB)
    The most up-to-date ADF70xx software download is bundled with all documentation, including schematics, for the ADF70xx family of transceivers. Layout can be found in the gerber files under the documentation tab.
FAQs/RAQs (1)
Overview (3)
Packages Application Notes (1)
Recommended Reading (1)
Software and Tools (5)
  • ADF70xx Evaluation Software  (zip, 24777 kB)
    The most up-to-date ADF70xx software download is bundled with all documentation, including schematics, for the ADF70xx family of transceivers. Layout can be found in the gerber files under the documentation tab.
  • ADF7xxx Device Driver Codes - Blackfin  (zip, 6 kB)
    Provides the c code source files allowing configuration using the ADSP-BF53X, Blackfin DSP processor. Routines to write the configuration values are provided as well as routines allowing a simple RF link to be setup between two ADF7020 devices. Please refer to application note, AN-771, for details on the hardware connections.
  • ADF7xxx Device Driver Codes - Microconverter  (zip, 15 kB)
    Provides the c code source files allowing configuration using an 8052 based microcontroller. Routines in this file will have to be adapted depending on the MCU and compiler used. This version uses the ADuC845/ADuC847 Microconverter from Analog Devices. The code was developed using the Keil C51 compiler within their uVision IDE.
  • ADIismLINK Development Platform  (zip, 24781 kB)
  • ADIsimSRD Design Studio
    Analog Devices ADIsimSRD Design Studio is a very powerful tool allowing real-time simulation and optimization of many of the parameters in a typical wireless system using the ADF7xxx family of transceivers and transmitters.
Software Configurable Products (1)
Solutions Bulletins (1)
User Guides (2)
Utilities and Conversions (1)
Webcasts (2)
Send Feedback X
content here.
content here.

Send Feedback

Close