![]() USB Isolation Reference CircuitsADI engineers have built, tested, and verified Circuits from the Lab™ reference circuits to address today's common design challenges, such as how to easily implement USB isolation in a system. Detailed circuit documentation is available which describes the circuit's function and benefit, and includes evaluation and test data. View the complete collection of Reference Circuits. |
D+/D- Bidirectional Isolation USB 2.0 Compliance Reinforced Isolation, up to 5kV rms isolation rating |
![]() |
-
USB Hub Isolation Circuit

This circuit isolates a hub as if it were a full speed peripheral device. The hub or host function requires that 2.5 W of power be available to each downstream port. Power to run the downstream side of the isolator and power the hub and ports is provided as part of the solution.
Read more, download design files, and evaluate circuit CN0158.
-
USB Cable Isolation Circuit

This circuit isolates a peripheral device that already implements a USB interface. While not meeting all requirements of the USB standard, it will provide a convenient isolated USB cable solution that provides power to the peripheral as well as operation at a fixed speed.
Read more, download design files, and evaluate circuit CN0159.
-
USB Peripheral Isolation Circuit

This circuit isolates a peripheral device that already
supports a USB interface. Because the peripheral is
not explicitly defined in this circuit, power to run
the secondary side of the isolator has been provided
as part of the solution.
Read more, download design files, and evaluatecircuit CN0160.

D+/D- Bidirectional Isolation