Low-Power, Unity-Gain Difference Amplifier Implements Low-Cost Current Source

In “Difference Amplifier Forms Heart of Precision Current Source,” published in Analog Dialogue in September 2009, the AD8276 unity-gain difference amplifier and AD8603 micropower op amp implement a precision current source. Figure 1 shows how the circuit can be simplified for use in low-cost, low-current applications.

Figure 1
Figure 1. Simple current source for low-cost and low-current applications.

The output current, IO, is approximately equal to the differential input voltage, VIN + – VIN–, divided by R1, as shown in the following derivation.

Equation 1
Equation 2
Equation 3

Thus, the differential input voltage appears across R1.

 Equation 4

Experimental Setup

  1. AD5750EVB (AD5750 driver and AD5662 16-bit nanoDAC®) provides a bipolar input to the AD8276.
  2. OI-857 multimeter measures input voltage, output voltage, and resistance.
  3. The nominal values of R1 and RLOAD are 280 Ω and 1 kΩ, respectively; the measured values are 280.65 Ω and 997.11 Ω, respectively.
  4. The output current is calculated by dividing the measured voltage by RLOAD.
Figure 2
Figure 2. Ideal and real output current vs. differential input voltage.

Experimental Results

Figure 2 shows the output current vs. the input voltage. The differential input voltage, which varies from –3.2 V to +3.2 V, is plotted on the X-axis; the output current is plotted on the Y-axis. The four lines show the ideal current and the real outputs at –40°C, +25°C, and +85°C.

Figure 3 shows the output current error vs. the input voltage. The three lines show the error at –40°C, +25°C, and +85°C.

Figure 3
Figure 3. Output current error vs. input voltage.

The real output current is limited by the short-circuit output current of the AD8276, as shown in Figure 4. Here, the short-circuit current is about 8 mA at –40°C.

Figure 4
Figure 4. AD8276 short-circuit output current vs. temperature.


By removing the external boost transistor and buffer and adding a single resistor, one can use the AD8276 to construct a low-cost, low-current source with a total error less than about 1.5% over the –40°C to +85°C temperature range. The output current range over temperature is about –11 mA to +8 mA when powered with a ±15-V supply. A unipolar source could be created with a single +5 V supply.


David Guo

David Guo

David Guo 是ADI公司位于北京的中国应用支持部门的一名现场应用工程师。获得北京理工大学机电工程硕士学位后,他在长峰集团工作过两年,担任导航终端硬件工程师。他于2007年加入ADI公司。