新闻

联络 Joy Zhao

ADI用于Microsemi SiC功率模块的隔离驱动器板加快产品上市时间

2018-03-07 - 中国,北京
  • Analog Devices, Inc. (ADI)与Microsemi Corporation 近日联合推出市场首款用于半桥SiC功率模块的高功率评估板,在200kHz开关频率时该板提供最高1200V电压和50A电流。隔离板的设计旨在提高设计可靠性,同时减少创建额外原型的需求,为电源转换和储能客户节省时间、降低成本并缩短上市时间。ADI公司和Microsemi将在2018年3月4日至8日于美国得克萨斯州圣安东尼奥举行的APEC 2018展会上展示该评估板。



    新评估板可用作更复杂拓扑(例如全桥或多电平转换器)的构建模块,以便对客户解决方案进行完整的工作台调试。它还可用作最终评估平台或用在类似转换器的配置中,以全面测试和评估ADI公司采用iCoupler®数字隔离技术的ADuM4135隔离栅极驱动器和高功率系统中的LT3999 DC-DC驱动器。


    该高功率评估板使得Microsemi的SiC 功率模块能够提供诸多优势,例如:通用测试台,提供更高功率密度以缩减尺寸和成本,通过隔离导电衬底和最小寄生电容实现更高的效率、性能和出色的热管理。这些特性使该评估板适合很多应用,包括电动汽车(EV)充电、混合动力汽车(HEV)/EV车载充电、DC-DC转换器、开关电源、高功率电机控制和航空作动器系统、等离子/半导体制造设备、激光和焊接、MRI和X光设备。


    产品聚焦


    • 半桥拓扑
    • 1200 V, 50 A@ 200 kHz
    • >100 kV/µs CMTI
    • 1.2 kV电气隔离
    • 独立的高端和低端PWM输入(单一控制,70 ns死区用于测试)
    • 1 LT3999 + 1 ADuM4135(高端和低端)
    • 全面测试的去饱和保护
    • 用于V+、V-和AC相位连接的低电感和高电流端子
    • 支持标准SP1封装的Microsemi半桥SiC功率模块,即APTMC120AM20CT1AG和APTMC120AM55CT1AG

    报价与供货
    产品 供货 起始单价 封装
    EV-MS4135PL1Z-UI 请通过电子邮件咨询工厂: RenwBoards@analog.com. 495美元 评估板
  • 关于ADI公司
    • Analog Devices (Nasdaq: ADI)是全球领先的高性能模拟技术公司,致力于解决最艰巨的工程设计挑战。凭借杰出的检测、测量、电源、连接和解译技术,搭建连接现实世界和数字世界的智能化桥梁,从而帮助客户重新认识周围的世界。
      详情请浏览ADI官网 www.analog.com/cn 。


  • 关于Microsemi


    Microsemi Corporation为航空航天、防务、通信、数据中心和工业市场领域提供全面的半导体和系统解决方案组合。产品包括:高性能和抗辐射的模拟混合信号集成电路、FPGA、SoC和ASIC;电源管理产品;计时和同步器件以及精密时间解决方案,为世界制定时间标准;语音处理器件;RF解决方案;分立元件;企业存储和通信解决方案、安全技术和可扩展防篡改产品;以太网解决方案;以太网供电IC和中跨设备;以及定制设计能力和服务。Microsemi总部位于美国加利福尼亚州亚里索维耶荷,在全球拥有约4800名员工。欲了解更多信息,请访问:www.microsemi.com.



    Microsemi和Microsemi徽标是Microsemi Corporation和/或其附属公司的注册商标或服务标志。本文提及的第三方商标和服务标志属各自所有人所有。


    Forward Looking Statements


    This press release contains forward-looking statements, which address a variety of subjects including, for example, the expected release date and availability, and expected benefits and performance of the new evaluation board product. Statements that are not historical facts, including statements about our beliefs, plans and expectations, are forward-looking statements. Such statements are based on current expectations and are subject to a number of factors and uncertainties, which could cause actual results to differ materially from those described in the forward-looking statements. For additional information about factors that could cause actual results to differ materially from those described in the forward-looking statements, please refer to recent filings with the Securities and Exchange Commission, including the risk factors contained in the most recent Quarterly Reports on Form 10-Q and/or Annual Reports on Form 10-K, made by Analog Devices and/or Microsemi.

  • 联络方式
与我们保持联络