|
Integer-N Software (ADF411X, ADF421X)
Evaluation Board Software
(zip, 4.74 MB)
The Evaluation Board Software (Rev 5.0), controls the operation of the Integer-N Synthesizer Evaluation Boards. The software is in zip format. Right click on the icon and choose "Save Link As" (Netscape Navigator) or "Save Target As" (Internet Explorer). Once the zip file has been stored locally, it can be extracted and the setup run by clicking on "setup.exe". Note that full data sheets for the synthesizers and technical notes for the evaluation boards are included in the zip file.
Ensure you uninstall any old versions of the software before installing the latest version.
Fractional-N Software (ADF4153, ADF4154, ADF4156, ADF4251, ADF4252)
Evaluation Board Software
(zip, 4.48 MB)
The Evaluation Board Software (Rev 3.0), controls the operation of the Fractional-N Synthesizer Evaluation Boards. The software is in zip format. Right click on the icon and choose "Save Link As" (Netscape Navigator) or "Save Target As" (Internet Explorer). Once the zip file has been stored locally, it can be extracted and the setup run by clicking on "setup.exe". Note that full data sheets for the synthesizers and technical notes for the evaluation boards are included in the zip file. Also note that when using Windows NT/2000 systems, installation must be done with administrator access.
Ensure you uninstall any old versions of the software before installing the latest version.
ADF4360 Family Software (ADF4360-X)
Evaluation Board Software
(zip, 7,856,373 bytes)
The ADF4360 Family Evaluation Board Software (Version 2.0), controls the operation of the ADF4360 Family Evaluation Boards. The software is in zip format. Right click on the icon and choose "Save Link As" (Netscape Navigator) or "Save Target As" (Internet Explorer). Once the zip file has been stored locally, it can be extracted and the setup run by clicking on "setup.exe". Note that full data sheets for the synthesizers and technical notes for the evaluation boards are included in the zip file.
Ensure you uninstall any old versions of the software before installing the latest version.
ADF4193 Software
Evaluation Board Software
(zip, 4.83 MB)
The Evaluation Board Software (Rev 4.3), controls the operation of the ADF4193 Synthesizer Evaluation Boards. The software is in zip format. Right click on the icon and choose "Save Link As" (Netscape Navigator) or "Save Target As" (Internet Explorer). Once the zip file has been stored locally, it can be extracted and the setup run by clicking on "setup.exe". Note that when using Windows XP/NT/2000 systems, installation must be done with administrator access.
Ensure you uninstall any old versions of the software before installing the latest version.
Loop Filter Software ADIsimPLL is a new design and simulation tool for Phase Locked Loops, using the ADI family of PLL synthesizers.
|