|
Shaker with reference device
An AC test that can be done at various frequencies
Required a calibrated reference device
Can test to higher g levels than 1g
Fixturing can be an issue for higher g levels
Gravity Test
Test sensor at +1g and -1g to calibrate offset and sensitivity using Earth's gravity
No need to calibrate the reference!
Fairly insensitive to alignment errors
Only works for DC sensors
Will not test the full scale of a high g device.
Gravity test method
Rotate the accelerometer at least 180° normal to the axis of sensitivity
Look for the minimum and maximum values
Zero g output = (maxout+minout)/2
Scale = (maxout-minout)/2 Volts per g
Calibration can be performed by the system microcontroller
Easy fixture construction
Dual axis accelerometers can calibrate both axis by extending the rotation to at least 360°
|